1. Home
  2. /
  3. Press Release
  4. /
  5. Heilind Now Stocking Molex’s Micro-Lock Plus Off-the-Shelf Discrete...

Heilind Now Stocking Molex’s Micro-Lock Plus Off-the-Shelf Discrete Wire Cable Assemblies

Micro-Lock Plus Off-the-Shelf Discrete Cable Assemblies are available in a variety of cable lengths and offer ready-to-use plug-and-play connections

WILMINGTON, Mass. (PRWEB) February 05, 2018 — Heilind Electronics, a leading global distributor of electronic components and authorized distributor for Molex, has expanded its selection of interconnect solutions with the company’s Micro-Lock Plus off-the-shelf discrete wire cable assemblies. Featuring up to a 1.5 A current rating, these assemblies come in a variety of cable lengths and use a compact connector to support both prototyping and global production.

Prototyping cable assemblies requires tooling to crimp terminals, resulting in increased costs for compliance testing. Molex off-the-shelf standard cable assemblies help to reduce tooling start-up costs by providing a completed assembly that meets IPC (Institute for Printed Circuits) specification designs. The Micro-Lock Plus also provides a one-source solution that not only eliminates the need for customer drawings, but also the process of locating a supplier to build the assemblies.

A unique advantage of the Micro-Lock Plus is the pin-to-pin mapping from receptacle to PCB header; this facilitates ready-to-use plug-and-play connections. In addition, the 1.25 mm pitch form factor secures mating retention without sacrificing compactness.

The Micro-Lock Plus family is a versatile connection option ideal for automotive and industrial settings, particularly in tight spaces and high temperatures.

Visit Heilind’s website for more information about Molex Micro-Lock Plus Off-the-Shelf Discrete Cable Assemblies.

About Heilind Electronics
Heilind Electronics, Inc. is one of the world’s leading distributors of connectors, relays, sensors, switches, thermal management and circuit protection products, terminal blocks, wire and cable, wiring accessories and insulation and identification products. Founded in 1974, Heilind has locations throughout the U.S., Canada, Mexico, Brazil, Germany, Singapore, Hong Kong and China.

View the original press release